Use the Basic tab to configure the Interval trend log.
Interval trend log properties - Basic tab
Property |
Description |
Status |
Displays the status of the trend log. |
Enabled |
Displays True if the trend log is enabled. |
Logged variable |
Enter the variable you want to log. |
Delta |
Select the minimum value change that triggers a new record. For more information, see Interval Trend Log Delta . |
Activation variable |
Enter the variable that makes the trend log start recording values when the variable is True . For more information, see Trend Log Activation . |
Activation time |
Specify the time when the trend log is to start recording values. For more information, see Trend Log Activation . |
Interval |
Type how often to log the variable. The interval defines the time between two log records. |
Log size |
Select the number of records to store before old records are overwritten, including internal records generated by the trend log. For more information, see Log Record Storage . |
Clear when enabled |
Select True to clear the trend log when it is enabled. |