earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concept

Concept


Products: Automation Server, AS-B, AS-P, Project Configuration Tool
Functionalities: Basic Functionality
Product version: 1.8, 1.9
4/5/2017

SmartStruxure Server Device Replacement Using Restore Workflow

Use the workflow to duplicate the SmartStruxure server device from a backup set.

 
action_zoom_plus_stroke Duplicate SmartStruxure server device using restore flowchart

Duplicate SmartStruxure server device using restore flowchart

Copy SmartStruxure server device Backup Set to WorkStation

Save the most current backup set of the SmartStruxure server device that you want to replace to WorkStation.

For more information, see Saving a SmartStruxure Server Device Backup Set to Another Location .

Add new SmartStruxure server device to network and configure communication settings

Add the new SmartStruxure server device to the network and configure the IP address.

For more information, see Configuring a SmartStruxure Server Device to Use DHCP .

For more information, see Configuring the SmartStruxure Server Device IP Address .

Log on to SmartStruxure server device using WorkStation

For more information, see Logging on to WorkStation as a Building Operation User .

Import backup set

Import the backup set to the new SmartStruxure server device.

For more information, see Importing a Backup Set to SmartStruxure Server Device .

Restore new SmartStruxure server device using the imported Backup Set

Restore the new SmartStruxure server device using the imported backup set.

For more information, see Restoring the SmartStruxure Server .

Tip:

If the SmartStruxure server device does not go online, you can manually recreate the SmartStruxure server device or restore the connections between the Enterprise Server and the SmartStruxure server device. For more information, see SmartStruxure Server Device Remains Offline After Restore .

The Restore process automatically renames the SmartStruxure server device and specifies the objects and properties that the SmartStruxure server device uses to reestablish links and go online.

  • Restore
  • SmartStruxure Server Device Replacement Using Restore
  • Backup Sets
  • Saving a SmartStruxure Server Device Backup Set to Another Location
  • Configuring a SmartStruxure Server Device to Use DHCP
  • Configuring the SmartStruxure Server Device IP Address
  • Logging on to WorkStation as a Building Operation User
  • Importing a Backup Set to SmartStruxure Server Device
  • Restoring the SmartStruxure Server
  • SmartStruxure Server Device Remains Offline After Restore