earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concept

Concept


Products: Device Administrator, Enterprise Server, Function Block Editor, Graphics Editor, ​License Administrator, ​License Server, Script Editor, Software Administrator
Functionalities: Basic Functionality
Product version: 1.9
12/14/2016

Uninstallation

To uninstall a Building Operation product you use the Windows Add Remove Program tool. The Windows Add Remove Program tool permanently removes the Building Operation product from the computer or server.

Notice

Loss of data

Return all activated network licenses to the License Activation Server before uninstalling the License Server and License Administrator. Licenses cannot be returned without a License Administrator. For more information, see Removing a Local License or Returning a Network License .

Failure to follow these instructions can result in loss of data.

Notice

Loss of data

Back up the Enterprise Server before uninstalling the product. All​ user settings, database information, and system files related to this product are erased. Files and backups created by the user remain and are not erased. For more information, see Backing Up SmartStruxure Servers Manually .

Failure to follow these instructions can result in loss of data.

Client tools and language packages are uninstalled together with the uninstallation of WorkStation.

  • Backing Up SmartStruxure Servers Manually
  • Installation Overview
  • Removing a Local License or Returning a Network License
  • Uninstalling the Device Administrator
  • Uninstalling the License Server
  • Uninstalling the License Administrator
  • Uninstalling a Language Pack
  • Uninstalling WorkStation