The EcoStruxure Building Engage mobile application provides flexibility and convenience for today’s building occupants by enabling them to control comfort settings in an office or conference room from their smartphone.
The Engage mobile application enables control of room temperature, fan speed, lights, and blinds/shades directly from a smartphone. A user can manage these settings when the application is connected to the RP-C controller.
The Engage mobile application is free and available for download from Google Play and Apple App Store.
Simulate mode is available for users to see the capabilities and benefits of the application without connecting to the RP-C controller.
The Engage mobile application connects easily via BLE (Bluetooth Low Energy) to the RP-C controller. The application is compatible with RP-C (HVAC) and RP controller expansion modules (lights and blinds).
The comfort controls of the Engage mobile application can be included as a service in the higher-tier, paid Enterprise offer along with other Operations Technology (OT), Information Technology (IT), and Concierge services.
The Engage Enterprise mobile application delivers high-value services to occupants in commercial buildings to help them be more satisfied and productive in their work environment.
Services are configurable and can include exterior and indoor navigation, employee directory, room booking, access control, dining and catering, transportation, smart parking, and other resources - all conveniently accessed through an integrated and unified application experience. For more information on EcoStruxure Engage Enterprise, see se.com .
Hardware and software requirements | |
Hardware
|
Android phones
|
Apple iPhones
|
|
Operating systems
|
Android 5.0 (Lollipop) and later
|
Apple iOS 11 and later
|
|
Compatibility | |
RP-C communication
|
|
EcoStruxure Building Operation
|
version 3.1.2 and later
|
Connection security | |
The connection to the RP-C requires a secure device pairing pin code. It is the responsibility of the customer to ensure that the pin code is securely managed. | |
Installation | |
The Engage mobile application does not require a license for activation and is available at no cost to the user. The installation of the Engage mobile application requires a connection to Google Play or Apple App Store for download. |