49 Topic(s)
You change the user regional settings in WebStation so that it fits your region.
You change the user theme settings so that it fits your screen.
You change the user theme settings so that it suits your needs.
You change the default system regional settings in WebStation so that it fits your region.
Use the Date and time tab to configure the server to use an external NTP server and to configure a time zone.
Values in the EcoStruxure Building Operation software are stored in the EcoStruxure Building Operation database with all input decimals. If a stored value consists of more decimals than the operating system is defined to display, the value is rounded off according to the operating system settings before it is displayed in WorkStation.
Consistent date and timestamping across a network is critical for system wide access control, security, communications, scheduling, alarms, and events. Network time uses the NTP protocol that provides the correct current UTC time.
To adjust the automation server time, time zone, and DST, you have to access the automation server through a WorkStation.
Use the Select Unit dialog box to define the unit and metric prefix of a value.
You can establish a lead and shadow relationship to synchronize the time on all your EcoStruxure BMS servers with the same network time server. The Date and Time object on the lead server contains the network time server addresses that are inherited by shadow servers.