191 Topic(s)
When you configure a schedule that controls events in a single part of a building, you might also want the same events to occur in other areas of the building. You can establish a lead and shadow relationship to synchronize the events in schedules and dates in calendars.
You configure a schedule as a shadow to synchronize it with a schedule that already contains all weekly events and exception events.
You configure a calendar as a shadow to synchronize it with a calendar that already contains all exception dates, date ranges, or calculated dates, such as a holiday calendar.
The EcoStruxure Building Operation software gives you a number of functions to monitor and manage your facilities.
Use the Add schedule event screen to select the type of schedule event.
An exception event occurs instead of the scheduled weekly events for a single date, date range, calculated date, or calendar.
Use the device detail screen to interact with the device and its features.
You remove unused schedules from a Multi schedule viewer.