37 Topic(s)
SpaceLogic Sensor devices are modular and are ordered in two parts: the sensor base and the cover. Four SpaceLogic communicating sensor base models are available as well as a variety of covers.
SpaceLogic Sensors are a family of living space sensors designed for BACnet/IP controllers using the EcoStruxure Building Operation user interface. These sensors use an RJ-45 sensor bus that provides communication and power from the BACnet/IP controller.
The Touchscreen Display model provides a menu-driven interface with a front menu and a functions menu screen that you configure through EcoStruxure Building Operation.
In the SpaceLogic Sensor 3-Button Cover model, you override the living space occupancy setting, for example, so an after-hours occupant can change the control setting to improve their comfort level. You enable occupancy override and also use the current occupancy value to control applications using the Display object Occupancy override property.
In the SpaceLogic Sensor Touchscreen Display model, you select the degree type in order to see the temperature in the preferred units of the room occupant. You enable this feature by choosing the Display object Allow temperature unit changes property, followed by the Temperature units property and its Fahrenheit or Celsius option.
In the SpaceLogic Sensor Touchscreen model, you select the fan speed to change the air flow in the designated living space. You enable this feature using the Display object Allow fan speed changes property.
You can program lighting control to create special scenes that illuminate an area based on the time of day, such as dimming the lights with the click of the night light button.
The 3-Button Cover model contains a passive, infrared sensor for occupancy detection and a plus and minus button to adjust the temperature setpoint. There is also an occupancy override button should the room occupant wish to confirm their presence, turn on the lights, and change the setpoint to a comfortable level.
Use the SpaceLogic Sensor LCD Temperature Sensor model Default screen to advance through the menus, increase and decrease temperature, change modes and degree types, and perform occupany overrides.
Use the SpaceLogic Sensor LCD Temperature Sensor model Degree Type screen to view and configure the degree type setting.