14 Topic(s)
The Schneider Electric SpaceLogic hardware devices for the EcoStruxure BMS include terminal bases, PS-24V power supplies, Central IO modules, automation servers such as AS-P servers and AS-B servers, BACnet/IP devices such as MP-C controllers, MP-V controllers, IP-IO modules, and RP-C controllers, RP controller expansion modules, remote control, KNX Modbus gateway, Bluetooth adapter, Wireless Adapter - Advanced, SpaceLogic Sensor devices, Advanced Display devices, and Operator Display devices.
Advanced Display v3 (AD v3) is the successor to AD v2. AD v3 provides an industrial grade Human Machine Interface (HMI), with battery-free power supply, for local access to the EcoStruxure BMS servers.
You connect AD v3 to an automation server in order to communicate with the automation server over a wired (USB) connection. You connect AD v3 to a 24 VDC power supply in order to supply AD v3 with power. You use the Y-shaped cable (SXWADUSBC10002 or SXWADUSBC10003) to connect AD v3 to both the automation server and the power supply.
AD v3 uses a wired (USB) connection to communicate with automation servers and the device must be powered by a 24 VDC power supply.
You install AD v3 on a control cabinet to use AD v3 for locally accessing the automation servers.
AD v3 has a power button that is used to power on the device, to turn off or reboot the device, and to perform other actions.
This section provides information on regulatory and agency compliance and approvals for the Advanced Display v3 (AD v3).
You perform a recovery (factory reset) of AD v3 to restore the device to factory default settings.