After licenses are activated on the License Server, you configure the Enterprise Server connection to the License Server. The address to the License Server is defined either during the installation of Enterprise Server, through License Administrator, or Windows registry.
Enterprise Server configuration and check out/in of Enterprise Server network license
Number |
Description |
1 |
Configure the Enterprise Server address to the License Server. |
2 |
Remove any activated local licenses. |
3 |
When the Enterprise Server starts, it automatically checks out an Enterprise Server network license from the License Server. |
When the Enterprise Server starts, it automatically checks out an available network license from a License Server. A checked out network license is not physically moved to or activated on the Enterprise Server. The license remains in the License Server but is allocated to the dedicated Enterprise Server. The license is therefore not available for other SmartStruxure servers to check out.
If the Enterprise Server does not start, refer to the Enterprise Server log for more information. For more information, see Viewing Enterprise Server System Log .