Use the Menu bar to access the different file menus in WorkStation.
Menu bar
Component |
Decription |
File |
Click to open the File menu, where you log off from the system, import and export information, print, and create new objects. For more information, see File Menu . |
Edit |
Click to open the Edit menu, where you edit objects in the system. For more information, see Edit Menu . |
View |
Click to open the View menu, where you display or hide Workspace components. For more information, see View Menu . |
Actions |
Click to open the Actions menu, where you carry out commands for objects selected in the System Tree pane or List View. For more information, see Actions Menu . |
Window |
Click to open the Window menu, where you close or navigate between open windows. For more information, see Window Menu . |
Tools |
Click to open the Tools menu, where you open the Control Panel and the Options dialog box. For more information, see Tools Menu . |
Help |
Click to open the Help menu, where you access the Building Operation help and view information about the WorkStation version number. For more information, see Help Menu . |