earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
How to

How to


Products: WorkStation
Functionalities: Basic Functionality
Product version: 1.3, 1.4, 1.5, 1.6, 1.7, 1.8, 1.9
7/2/2013

Selecting a Default Workspace

You select the workspace that you want to use when you log on to WorkStation for the first time.

Show More
action_close

The workspace in WorkStation and WebStation is the area where you perform all tasks at your site, such as acknowledging alarms and viewing trend logs.

The workspace is made up of different components, such as panes, lists, and views. These components can be configured in a number of different ways. You can hide or display components and create and save your own workspace. You can also reset the workspace layout to the default layout for the user group your user account belongs to.

WebStation uses cookies to remember your workspace when you log off. When you log on again, you get the workspace you used when you logged off. If you clear your web browser, you will regain the default workspace.

 
action_zoom_plus_stroke Workspace in WorkStation (left) and WebStation (right)

Workspace in WorkStation (left) and WebStation (right)

Some objects have specific views in WorkStation and WebStation:

  • Alarms

  • Documents

  • Graphics (TGML)

  • Events

  • Trend Charts

  • Trend Log Lists

  • Schedules

  • Calendars

  • Watch

When you open an object that does not have a specific view, the Properties dialog box for that object is displayed.

Panels

Panels are a way to create workspaces that display two or more components in Building Operation, for example graphics, trend charts, trend list and alarm views.

For more information, see Panels .

Web Pages

Web pages on the Internet can be displayed in the Workspace in Building Operation.

For more information, see Web Pages .

To select a default workspace
  • In WorkStation , in the Select Default Workspace dialog box, click the workspace you want to use as your default workspace.

     
    action_zoom_plus_stroke

The selected workspace is your default workspace the next time you log on to WorkStation.

  • Log on to WorkStation or WebStation
  • Logging on to WorkStation as a Building Operation User
  • Saving Log On Details
  • Workspaces
  • Switching Workspaces
  • Logging Off WorkStation
  • Exiting WorkStation
  • Changing Your Password
  • Building Operation WorkStation Window