122 Topic(s)
Part numbers: SXWIPIOAA10001, SXWIPIOBA10001, and SXWIPIOCA10001
There are three LEDs on the front panel of the IP-IO module.
The Status LED on the front of the automation devices changes color and flashes to indicate the status of the device.
BACnet/IP devices have three types of memory:
The wiring recommendations for the communication ports on the automation servers, BACnet/IP devices, RP controller expansion modules, and Operator Display devices apply to wires and cables used for RS-485 communications, LonWorks communications, USB connections, Ethernet connections, sensor bus connections, room bus connections, and RP controller Modbus network connections. Always use the recommended cables and wires.
There are many different kinds of external devices from different vendors that can be connected to an EcoStruxure BMS.
The override display has a menu-driven user interface, which facilitates overriding of the outputs, local configuration of inputs and outputs, and other tasks.
You log on to the Commission mobile application to perform commissioning, flow balance, and checkout operations on BACnet/IP controllers.
You can select the Feedback option to rate your experiences and provide detailed information on the Commission mobile application.
The Schneider Electric SpaceLogic hardware devices for the EcoStruxure BMS include terminal bases, PS-24V power supplies, Central IO modules, automation servers such as AS-P servers and AS-B servers, BACnet/IP devices such as MP-C controllers, MP-V controllers, IP-IO modules, and RP-C controllers, RP controller expansion modules, remote control, KNX Modbus gateway, Bluetooth adapter, Wireless Adapter - Advanced, SpaceLogic Sensor devices, Advanced Display devices, and Operator Display devices.