earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concept

Concept


Products: AS-B, IP-IO , MP-C
Functionalities: Hardware
Product version: 3.3, 2022
8/15/2022

User Experience

The override display has a menu-driven user interface, which facilitates overriding of the outputs, local configuration of inputs and outputs, and other tasks.

The main screens of the user interface are briefly described below.

Home screen

The Home screen is displayed when the device is powered on. To go to the next screen, press the Enter key

 
action_zoom_plus_stroke
.

 
action_zoom_plus_stroke Home screen (AS-B server example)

Home screen (AS-B server example)

For more information, see Home Screen on AS-B Servers .

For more information, see Home Screen on MP-C or IP-IO Module .

I/O Filter screen

The I/O Filter screen provides an overview of the number of I/O points and enables you to filter the I/O List screen on inputs, outputs, and overriden outputs.

 
action_zoom_plus_stroke I/O Filter screen

I/O Filter screen

For more information, see I/O Filter Screen .

I/O List screen

The I/O List screen presents the I/O points in a list. You use the screen to view an I/O point, to select an output that you want to override, or to select an I/O point to be locally configured.

 
action_zoom_plus_stroke I/O List screen

I/O List screen

For more information, see I/O List Screen .

Output Override screen

The Output Override screen enables you to manually override an output and to remove an override for an output. The screen looks similar for the different types of outputs.

 
action_zoom_plus_stroke  Output Override screen

Output Override screen

For more information, see Output Override Screen .

I/O Configuration screen

The I/O Configuration screen is the starting point to locally configure inputs and outputs. To make this screen appear, press and hold down Home key

 
action_zoom_plus_stroke
for three seconds.

 
action_zoom_plus_stroke I/O Configuration screen (AS-B server example)

I/O Configuration screen (AS-B server example)

For more information, see I/O Configuration Screen .

  • AS-B Servers
  • MP-C Controllers
  • Output Override Function
  • Home Screen on AS-B Servers
  • Home Screen on MP-C or IP-IO Module
  • I/O Filter Screen
  • I/O List Screen
  • Output Override Screen
  • I/O Configuration Screen
  • Icons
  • Keys