141 Topic(s)
You must configure a unique MS/TP address for the RP and MP controllers that support MS/TP communications. You do so during installation by using position 1-7 on the address DIP switch.
Part numbers: SXWMPC15A10001, SXWMPC18A10001, SXWMPC18B10001, SXWMPC24A10001, and SXWMPC36A10001
There are five LEDs on the front panel of the MP controller.
The Status LED on the front of the automation devices changes color and flashes to indicate the status of the device.
BACnet/IP devices have three types of memory:
The wiring recommendations for the communication ports on the automation servers, BACnet/IP devices, RP controller expansion modules, and Operator Display devices apply to wires and cables used for RS-485 communications, LonWorks communications, USB connections, Ethernet connections, sensor bus connections, room bus connections, and RP controller Modbus network connections. Always use the recommended cables and wires.
There are many different kinds of external devices from different vendors that can be connected to an EcoStruxure BMS.
The MP controller sensor bus allows SpaceLogic Sensor devices to be connected to the controller.
The override display has a menu-driven user interface, which facilitates overriding of the outputs, local configuration of inputs and outputs, and other tasks.
You log on to the Commission mobile application to perform commissioning, flow balance, and checkout operations on BACnet/IP controllers.