earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
How to

How to


Products: RP-C
Functionalities: Hardware
Product version: 2022
4/5/2022

Powering Up an RP-C 230 V Controller Model

You perform the following steps to power up an RP-C 230 V controller model.

Show More
action_close

The RP-C can be installed on a DIN rail or flat surface.

Rules and regulations

The RP-C must be professionally installed to comply with the following rules and regulations:

  • Part 15 of the Federal Communications Commission (FCC) rules

  • Innovation, Science and Economic Development Canada (ISED) licence-exempt Radio Standards Specifications (RSSs)

  • 2014/53/EU Radio Equipment Directive (RED) of the European Union (EU)

  • S.I. 2017/1206 - Radio Equipment Regulations 2017 of the United Kingdom (UK)

For more information, see RP-C Regulatory Compliance and Approvals .

The RP-C and its antenna(s) must be installed to provide a separation distance of at least 20 cm (8 in.) from all persons and must not be co-located or operating in conjunction with any other antenna or transmitter. Information on recommended RF exposure limits can be obtained from Health Canada's website, www.canada.ca/en/health-canada .

Installation orientation restrictions

The restrictions on installing the device in other orientations differ between the different RP-C controller models. For more information, see RP-C Models .

Notice

CONTROLLER DAMAGE

Follow the installation orientation restrictions that apply to the specific RP-C controller model.

Failure to follow these instructions can result in equipment damage.

Installation orientation restrictions for RP-C 24 V controller models

Under normal operating conditions of 0 to 50 °C (32 to 122 °F), the RP-C 24 V controller models can be installed in the following orientations:

  • Horizontally (on a DIN rail going from left to right), with the device label text in the upright position reading left to right. See “a” in the following figure.

  • Vertically (on a DIN rail going from top to bottom), which means that the device is rotated +90 degrees or -90 degrees from the horizontal position. See “b” and “c” in the following figure.

  • Face down from a ceiling. See “d” in the following figure.

  • Face up on a horizontal surface. See “f” in the following figure.

The only installation orientation that is not supported for the RP-C 24 V controller models is when the device is rotated 180 degrees from the horizontal position, that is, with device label text up and down. See “e” in the following figure. In the up and down position, the controller's thermal specifications may be exceeded, which can damage the controller.

 
action_zoom_plus_stroke Installation orientation restrictions for RP-C 24 V controller models operated in normal conditions, 0 to 50 °C (32 to 122 °F)

Installation orientation restrictions for RP-C 24 V controller models operated in normal conditions, 0 to 50 °C (32 to 122 °F)

When the RP-C 24 V controller models are used for rooftop applications, -40 to +60 °C (-40 to +140 °F), the device should be installed horizontally, with the device label text in the upright position reading left to right. See “a” in the following figure. Any other installation orientation (“b”, “c”, “d”, “e”, and “f” in the figure) may exceed the controller's thermal specifications, which can damage the controller.

 
action_zoom_plus_stroke Installation orientation restrictions for RP-C 24 V controller models operated at -40 to +60 °C (-40 to +140 °F)

Installation orientation restrictions for RP-C 24 V controller models operated at -40 to +60 °C (-40 to +140 °F)

Installation orientation restrictions for RP-C 230 V controller models

Under normal operating conditions of 0 to 50 °C (32 to 122 °F), the RP-C 230 V controller models can be installed in the following orientations:

  • Horizontally (on a DIN rail going from left to right), with the device label text in the upright position reading left to right. See “a” in the following figure.

  • Vertically (on a DIN rail going from top to bottom), which means that the device is rotated +90 degrees or -90 degrees from the horizontal position. See “b” and “c” in the following figure.

Installing the RP-C 230 V controller models rotated 180 degrees from the horizontal position is not supported. See “e” in the following figure. Installing the RP-C 230 V controller models face down from a ceiling (“d” in the figure) or face up on a horizontal surface (“f” in the figure) is only supported in the operating temperature range 0 to 40 °C (32 to 104 °F), but not in the temperature range 0 to 50 °C (32 to 122 °F). Installing the controller in an orientation that is not supported may cause the controller's thermal specifications to be exceeded, which can damage the controller.

 
action_zoom_plus_stroke Installation orientation restrictions for RP-C 230 V controller models operated in normal conditions, 0 to 50 °C (32 to 122 °F)

Installation orientation restrictions for RP-C 230 V controller models operated in normal conditions, 0 to 50 °C (32 to 122 °F)

Installation on a DIN rail

A DIN rail is a common and convenient technique for installing the RP-C controller along with other associated control and monitoring devices. The most efficient ventilation is achieved with the wall-mounted DIN rail oriented horizontally and with adequate space provided between the RP-C rail and adjacent rails or other devices.

The RP-C controller is typically installed horizontally (on a DIN rail going from left to right), with the device label text in the upright position reading left to right.

 
action_zoom_plus_stroke Example of an RP-C controller installed on a horizontal DIN rail

Example of an RP-C controller installed on a horizontal DIN rail

Installation in a cabinet
 
action_zoom_plus_stroke RP-C controllers installed on horizontal DIN rails in a cabinet

RP-C controllers installed on horizontal DIN rails in a cabinet

When installing RP-C controllers in a cabinet, it is recommended to provide ample space between the DIN rails and controllers for sufficient ventilation.

DIN rail end clip

To help prevent the device from sliding down or sideways on the DIN rail, install an end clip for DIN 35 (part number SXWDINEND10001) tightly against the bottom or rightmost device on the rail. The end clip is easily removed if you bend the snap lock open with a screwdriver.

Notice

CONTROLLER DEVICE DAMAGE

Use an end clip (part number SXWDINEND10001) when you install the BACnet/IP Controller device on a vertical DIN rail.

Failure to follow these instructions can result in equipment damage.

 
action_zoom_plus_stroke End clip for DIN 35 fixed across the DIN rail

End clip for DIN 35 fixed across the DIN rail

Screw terminals

All RP-C controller models have fixed screw terminals.

Anchor points for cable ties

The RP-C controller has four anchor points that can be used to fasten cable ties or other accessories for bundling wires.

 
action_zoom_plus_stroke Anchor points for cable ties

Anchor points for cable ties

Optional covers

All RP-C controller models can be equipped with optional covers to reduce access to the screw terminals and wires if desired.

 
action_zoom_plus_stroke Optional covers

Optional covers

Show More
action_close

The RP-C controller comes in six different models, which offer five different combinations (sets) of I/O point types and CPU types. Four of the RP-C controller models support 24 VAC/DC input power and two of the models support 230 VAC.

  • RP-C 24 V controller models:

    RP-C-12A-F-24V, RP-C-12B-F-24V, RP-C-12C-F-24V, and RP-C-16B-F-24V

  • RP-C 230 V controller models:

    RP-C-16A-F-230V and RP-C-16B-F-230V

 
action_zoom_plus_stroke RP-C model number structure

RP-C model number structure

Range

Model

I/O–CPU Set

I/O Points

CPU Type

RAM / Flash Memory

Input Power

Advanced

RP-C-12A-F-24V

12A

12

ARM Cortex-A7 single-core

6 MB / 48 MB

24 VAC at 50/60 Hz or 24 to 30 VDC

Advanced

RP-C-12B-F-24V

12B

12

ARM Cortex-A7 single-core

6 MB / 48 MB

24 VAC at 50/60 Hz or 24 to 30 VDC

Advanced

RP-C-12C-F-24V

12C

12

ARM Cortex-A7 single-core

6 MB / 48 MB

24 VAC at 50/60 Hz or 24 to 30 VDC

Advanced

RP-C-16A-F-230V

16A

16

ARM Cortex-A7 single-core

6 MB / 48 MB

230 VAC at 50/60 Hz

Pro

RP-C-16B-F-24V

16B

16

ARM Cortex-A7 dual-core

128 MB / 64 MB

24 VAC at 50/60 Hz or 24 to 30 VDC

Pro

RP-C-16B-F-230V

16B

16

ARM Cortex-A7 dual-core

128 MB / 64 MB

230 VAC at 50/60 Hz

For more information, see RP-C Onboard I/O .

For more information, see RP-C Built-in Power Supply .

All RP-C models have the same small footprint.

Differences Between RP-C Hardware Versions

There are a number of differences in hardware between different hardware versions of the RP-C-12A-F-24V, RP-C-12B-F-24V, RP-C-12C-F-24V, and RP-C-16A-F-230V controller models.

For more information, see Differences Between RP-C Hardware Versions .

Notice

CONTROLLER DEVICE DAMAGE

Ensure that the input power voltage level meets the specifications of the RP controller.

Failure to follow these instructions can result in equipment damage.

To power up an RP-C 230 V controller model
  1. Check that all wiring is correct.

  2. Ensure that appropriate cable strain relief is provided, especially for wires that carry 30 VAC or 42.4 VDC or above.

    You can use the anchor points on the controller enclosure and cable ties to fasten and fix the cables.

  3. Ensure that the 230 VAC at 50/60 Hz is supplied to terminals 1 (Line lead) and 2 (Neutral lead).

     
    action_zoom_plus_stroke
  4. Ensure that protective earth ground (PE) is connected to terminal 3

     
    action_zoom_plus_stroke
    . For the controller model RP-C-16A-F-230V, this instruction applies only for hardware version 10 and later of the controller.

    For more information, see Differences Between RP-C Hardware Versions .
    Tip:

    The hardware version is shown on the label on the side of the device. If the side of the device is not accessible, the text on the front can be used to identify the hardware version. For example, “SpaceLogic RP-C” is displayed on devices of hardware version 10 and later, while “SmartX IP Controller” is printed on devices of hardware version 9 and earlier.

  5. After powering up, check that the Status LED changes as follows:

    • Bluetooth interface enabled (default): Flashing blue/green light (Normal operation, Bluetooth advertising)

    • Bluetooth interface disabled: Constant green light, after about a minute (Normal operation, No Bluetooth activity)

    For more information, see RP-C LEDs .

  • RP-C Device Installation
  • RP-C Models
  • RP-C Screw Terminals
  • RP-C-16A-F-230V Screw Terminals
  • RP-C-16B-F-230V Screw Terminals
  • Differences Between RP-C Hardware Versions
  • RP-C LEDs
  • Status LEDs