Manual Backup is a non-automated process of copying and storing data on a selected EcoStruxure BMS server. You can use this option to create backups on an as-needed basis. You can also manually restore the data at any time.
You log on to one of the following EcoStruxure BMS servers to initiate a manual backup:
Backup Set Naming
For manual backups, the system initially names the backup set by combining the EcoStruxure BMS server name with the localized date and time of the machine running WorkStation. For scheduled backups, however, the system combines the EcoStruxure BMS server name with the UTC time in the backup set name rather than the local time.
Tip:
The system also retains the UTC time of manually generated backups. To view the UTC time rather than the localized time for a manual backup set, select the
Backup date
property from the column selector of the Backup Sets List view.
For more information, see Columns
.
If you log on to the Enterprise Server in WorkStation to create a backup of the automation server, the system automatically checks for identical backup set names. If a name is found in the
AS Archives
folder, the system warns of a potential duplication by highlighting the
Backup set name
prefix box or the
Backup set name
suffix box in solid red. If you do not change the prefix or suffix, the system displays a red box around the backup set in the
Backup set name
column to indicate that there is an existing name. If you still do not change the name, the system automatically appends an extended time stamp to prevent the accidental overwriting.
For more information, see Duplicate Backup Set Names in Multi-server Systems
.
Remote Backup and Restore of Automation Servers
When you log on to an Enterprise Server, you can perform remote backups of any automation server in the system. Whenever a backup occurs on the automation server, the system overwrites the locally stored file on the automation server with the new backup file. The Enterprise Server then retrieves and stores this backup file in a separate directory on the computer that runs the Enterprise Server.
For more information, see Remote Backup and Restore of Automation Servers
.
Local Backup of EcoStruxure BMS Servers using Device Administrator
You can manually create backup sets using Device Administrator. The backup sets can be saved at any location. One or many EcoStruxure BMS Servers can be backed up at the same time.
For more information, see Local Backup of EcoStruxure BMS Servers using Device Administrator
.