87 Topic(s)
You must configure a unique MS/TP address for the RP and MP controllers that support MS/TP communications. You do so during installation by using position 1-7 on the address DIP switch.
You configure the MP-V controller setpoints to set up the parameters by which the controller is flow balanced. These setpoints include the maximum flow setpoint, selected by default, and the intermediate and minimum flow setpoints, which are optional.
You log on to the Commission mobile application to perform commissioning, flow balance, and checkout operations on BACnet/IP controllers.
You can reset and restart the MP controllers in different ways depending on how long you press the reset button. The resets and restarts can affect the retention of values after restart based on the retain levels configured for the variables.
You can reset and restart the RP controllers in different ways depending on how long you press the reset button. The resets and restarts can affect the retention of values after restart based on the retain levels configured for the variables.
You can use the Commission mobile application to update or delete your Schneider Electric Identity Management System (IDMS) user profile on the Schneider Electric Exchange site.
You can commision an Insight-Sensor from the Commission mobile application.
Should you wish, you can change user settings in the Commission mobile application. This includes changing the in-application language and granting or denying access to system settings for the application location, camera, or storage.
SpaceLogic Sensors are a family of living space sensors designed for BACnet/IP controllers using the EcoStruxure Building Operation user interface. These sensors use an RJ-45 sensor bus that provides communication and power from the BACnet/IP controller.
You discover a device to add it to the list of available devices.