568 Topic(s)
The RP controller Modbus RTU (RS-485) subnetwork allows standard Modbus devices and the KNX Modbus gateway (RP-C-EXT-KNX) to be connected to the controller.
You add an Entitlement to get a list of the licenses that you can assign.
Use the Add Entitlement dialog box to add an entitlement to Device Administrator.
You add an Entitlement to get a list of the licenses that you can assign.
You connect RP controller expansion modules and multi-sensors to the RP-C room bus to provide the devices with power and communication from the RP-C controller.
The RP-C controllers can be reconfigured to communicate with automation servers based on the BACnet MS/TP protocol, instead of the BACnet/IP protocol.