earth_america
user_standard Log on
action_search_stroke
earth_america

BACnet/IP Devices

RP-C
MP-C
MP-V
IP-IO
MP-C Smoke Control
MP-V Smoke Control
IP-IO Smoke Control
Refine your search
arrow2_down
Refine your search
Ok
Ok
Ok

381 Topic(s)

Concept

The RP controller Modbus RTU (RS-485) subnetwork allows standard Modbus devices and the KNX Modbus gateway (RP-C-EXT-KNX) to be connected to the controller.

How to

You must configure a unique MS/TP address for the RP and MP controllers that support MS/TP communications. You do so during installation by using position 1-7 on the address DIP switch.

How to

You connect RP controller expansion modules and multi-sensors to the RP-C room bus to provide the devices with power and communication from the RP-C controller.

Concept

The RP-C controllers can be reconfigured to communicate with automation servers based on the BACnet MS/TP protocol, instead of the BACnet/IP protocol.

Specifications

Specifications

How to

You connect a Non-isolated RS-485 Adapter (via a separate connection cable) to a BACnet/IP controller to convert the controller RS-485 RJ45 interface to screw terminals, which is required to connect the controller to a BACnet MS/TP (RS-485) network. You use a Non-isolated RS-485 Adapter (SXWNISORS48510001) when the BACnet MS/TP network includes non-isolated controllers, such as the b3 BACnet family of zone controllers.

How to

You connect an Isolated RS-485 Adapter (via a separate connection cable) to a BACnet/IP controller to convert the controller RS-485 RJ45 interface to screw terminals, which is required to connect the controller to a BACnet MS/TP (RS-485) network. You use an Isolated RS-485 Adapter (SXWISORS48510001) when the BACnet MS/TP network is comprised of isolated controllers, such as MNB BACnet devices (zone controllers) and selected others.

Concept

The RP-C sensor bus allows SpaceLogic Sensor devices to be connected to the controller.

Concept

The RP-C provides the following combination of communication ports: