74 Topic(s)
You configure the MP-V controller setpoints to set up the parameters by which the controller is flow balanced. These setpoints include the maximum flow setpoint, selected by default, and the intermediate and minimum flow setpoints, which are optional.
You log on to the Commission mobile application to perform commissioning, flow balance, and checkout operations on BACnet/IP controllers.
You can select the Feedback option to rate your experiences and provide detailed information on the Commission mobile application.
The SpaceLogic Bluetooth Adapter is plugged into a SpaceLogic Sensor to provide a wireless Bluetooth connection to the BACnet/IP controller (Sensor Bus compliant controller) for commissioning, maintenance, and troubleshooting of the controller and the sensor.
You can use the Commission mobile application to update or delete your Schneider Electric Identity Management System (IDMS) user profile on the Schneider Electric Exchange site.
You commission the following Zigbee high security devices from the Commission mobile application when Zigbee network and logical devices are configured on your BACnet/IP controller:
You can commision an Insight-Sensor from the Commission mobile application.
Should you wish, you can change user settings in the Commission mobile application. This includes changing the in-application language and granting or denying access to system settings for the application location, camera, or storage.